Create MotorPanel instances
    Instantiate the MotorPanel type and create the required dynamic links.
- InProject view, right-clickMainWindow (type)and select twice.UnderMainWindow (type),MotorPanel1andMotorPanel2appear.
- SelectMotorPanel1and inProperties, create a dynamic link betweenMotorAliasand .For more information about dynamic links, see Create dynamic links.
- SelectMotorPanel2and inProperties, create a dynamic link betweenMotorAliasand .For more information about dynamic links, see Create dynamic links.
Based on the 
MotorAlias
 values, the MotorExt
 values are set automatically.Provide Feedback