Create Motor objects
    Create sample Motor object data to populate the list box and gauges.
- InProject view, right-clickModeland select .
- Hover-over the object, select, and enter Motor. Motor.
- Add and configure variables:- InProperties, at the top, add two variables by selectingand selecting Variable. Variable.
- Rename the variables by hovering-over each variable, selecting, and entering: - Speed
- Acceleration
 
 
- Convert the Model object into an object type:- InType view, double-clickModel.
- FromProject view, dragMotorintoType view.
 
- Create and organize Motor object instances:- InProject view, right-click theModelfolder and select .
- Hover-over the folder, select, and enter MotorObjects. MotorObjects.
- InProject view, dragMotorinto theMotorObjectsfolder.
- Create nine Motor object instances by draggingMotorfromType viewinto theMotorObjectsfolder inProject view.
 
- Configure each Motor instance:- InProject view, select a motor.
- InProperties, set theAccelerationandSpeedproperties values.You can enter any values of the valid type.For example, enter:PropertyValueAcceleration1Speed11
 
Provide Feedback