Develop alarm comment dialog box
    Develop a comment dialog box that allows you to enter a comment when you acknowledge
      an alarm in Alarm Summary. 
Application example

     NOTE: 
    
Download a sample project:
AlarmCommentBox.zipPrerequisites
- To develop the project
- Arrange the interface elements.
- Save the project.

Select  to run the project using the client
        emulator to test your project. To run the project on a remote client, see Add a target device.
  to run the project using the client
        emulator to test your project. To run the project on a remote client, see Add a target device.
Run
Provide Feedback