Create a project
    Create a Quick start project to develop your 
FactoryTalk Optix Application
.- OpenFactoryTalk Optix Studio.
- UnderCreate a new project, selectDefault.
- InName, enter the name of the project.For example, enterQuickStart
- (optional) InLocation, edit the directory in which you want to save the project.
- Verify thatUse version controlis selected.
- SelectCreate.
Provide Feedback