Import controller variables
    Configure a communication driver to import sample tags (controller variables) from a Logix controller.
     TIP: 
    Instead of importing controller variables from a Logix controller, you can create variables manually. See Create variables.
Prerequisites
In the Logix Designer application, download the LogixTags.ACD project to a physical Logix controller or an emulated 
FactoryTalk® Logix Echo™
 controller. Set the controller in the run mode.
        For more information, see the Logix Designer online help.
- To import controller variables
- From the toolbar, select.Open dashboard page
- In the editor, selectConfigure communications to devices.
- SelectNew stations.
- SelectRA EtherNet/IP Stationand selectNext.
- (optional) To import the controller tags in the online mode, inRoute, enterand selectIP_Address\Backplane\Chassis_Slot_NumberNext.TIP: For more information, see RA EtherNet/IP Driver.
- SelectNext.
- Fetch the controller tags:- To fetch the controller tags in the offline mode, selectBrowseand select the downloadedLogixTags.ACDfile.
- To fetch the controller tags in the online mode, select theOffline/Onlinetoggle to change it to theOnlineposition.
 
- Select all controller tags and selectNext.Selected tags in the online mode 
- SelectExit.
In 
Project view
, the imported controller variables are available in the  node. Note this location.Imported controller variables

Provide Feedback