Configure a recipe
    Create a recipe schema that uses the Ingredient01, Ingredient02, and Ingredient03 variables.
- From the toolbar, select.Open dashboard page
- In the editor, selectConfigure a recipe.
- SelectNew recipe.
- Create a dynamic link betweenTarget nodeand:- If you created variables, .
- If you imported Logix controller variables, .
 
- SelectNextand selectNext.
- SelectNew database.
- InName, enterRecipeDBand selectNext.
- SelectNextand selectNext.
- SelectIngredient01,Ingredient02, andIngredient03, and selectNext.Selected variables 
- SelectExit.
In 
Project view
, RecipeSchema1
 appears under Recipes
.Provide Feedback