FactoryTalk Optix Studio
    FactoryTalk Optix Studio
 is an integrated development environment with a framework of functional modules for designing and compiling HMI or Internet of Things (IoT) applications.FactoryTalk Optix Studio
 includes a library of predefined objects that support the modular design of graphical interfaces, features, and logic operations of an HMI application. By using specific C# language scripts, you can automate various actions in the design phase and add customized functions to projects.Desktop and web editors 
      FactoryTalk Optix Studio
 is available as a web and a desktop development environment that you use to build FactoryTalk Optix Applications
  and deploy them to client systems. You access FactoryTalk Optix Studio web editor
 through FactoryTalk Hub
.If there is an Internet connection outage:
        
- FactoryTalk Optix Studio web editortries to reconnect to the Internet every 5 seconds. During that period, you cannot interact withFactoryTalk Optix Studio web editor. OnceFactoryTalk Optix Studio web editorreconnects to the Internet, you can continue where you left off.
- FactoryTalk Optix Applicationdisplays the message "Server unreachable" after 10 seconds. When theFactoryTalk Optix Applicationreconnects to the Internet, the application attempts to restore the user session and the interface displays.
Provide Feedback