FactoryTalk Optix Studio CLI
    Use the command-line interface (CLI) of 
FactoryTalk Optix Studio
 to perform
            actions without having to interact with the graphical user interface (GUI).
     TIP: 
    Running CLI commands is useful for scripting and
            automating pipelines.
To run a command, see  Run a CLI command. To learn about the
            available commands, see CLI commands.
Provide Feedback