Network ports configuration
    Configure firewalls and ports to ensure successful communication. Review the default values for user-configurable ports and the comprehensive list of ports used by 
FactoryTalk Optix
 for inbound and outbound connections.
     TIP: 
    Ports 80 and 443 may be already configured for devices like OptixPanels and Embedded Edge Compute Module (EECM).
      
FactoryTalk Optix modules
      - WebPresentationEngine- Protocol: This port is configurable. If Protocol is blank, the port reflects the protocol configuration.- If set to HTTP: 80/TCP
- If set to HTTPS: 443/TCP
 
 
- ApplicationUpdateServer- Fixed Port: 49100/TCP
 
- Communication Drivers- RA Ethernet/IP Driver- Port: 44818/TCP
 
- Modbus- Port: 502/TCP
 
- Melsec FX3U: Configure the TCP port on PLC.- Default port: 1034/TCP
 
- Melsec Q: Configure the TCP port on PLC.- Default port: 1/TCP
 
- Omron Ethernet/IP- Port: 44818/TCP
 
- Omron FINS- Port: 9600/TCP
 
- S7 TCP- Port: 102/TCP
 
- S7 TIA- Port: 102/TCP
 
- TwinCAT- Port: 851/TCP
 
- CODESYS- Port: 1217/TCP
 
 
- DataStores- SQL/SQL Express- Port: 1433
 
- MySQL- Port: 3306
 
 
- User Authentication- LDAP: Configurable in the domain server address- Default port 39.
 
- AD: This port is configurable. If AD is blank, the port reflects the protocol configuration.- The default port is 39.
 
 
- OPC UA- Server: User-configurable- Default port: 59100/TCP
 
- Client- The port depends on source server configuration.
 
 
- FTRA Service- Ports: 5000/TCP, 14273/TCP, and 5936/TCP
 
- FT Hub- FactoryTalk Optix acts as a client, using a random port at every connection.
 
External modules from TemplateLibrary
      - MQTT (PushAgent and MQTTLogic):Configure these ports depending on the server configuration:- Standard: 1883/TCP
- Secure: 8883/TCP
 
- Email (AlarmsWithEmailNotification):Configure these ports depending on the server configuration:- SMTP- 57/TCP, 25/TCP, or 465/TCP
 
 
Provide Feedback