Licensing and accounts FAQs
    Which licenses do I need to create and deploy projects?
You can create and deploy projects by using FactoryTalk Optix Studio with some
                limitations. To use all deployment features, you need to purchase FactoryTalk Optix
                Studio Pro. See FactoryTalk Optix Installation Guide |
                    FactoryTalk Optix Studio versus FactoryTalk Optix Studio Pro. If you
                deploy a FactoryTalk Optix Application without licensing the target machine, the
                application will run for two hours before shutting down automatically.
What kind of software do I need to create and deploy projects?
You need FactoryTalk Optix Studio or FactoryTalk Optix Studio Pro to develop projects
                and FactoryTalk Optix Runtime Tools to run FactoryTalk Optix Applications on target
                devices. See FactoryTalk Optix Installation Guide.
How do I choose the right Runtime entitlement for my application?
To choose the right Runtime entitlement, see:
Where can I manage the FactoryTalk Optix Pro entitlement that I purchased?
                
See FactoryTalk Optix Installation Guide |
                    FactoryTalk Optix Sutdio Pro Upgrade and the subsequent topics. 
Where can I manage the FactoryTalk Optix Runtime entitlement that I purchased?
                
To purchase, allocate, activate, start and rehost the Runtime entitlement, see FactoryTalk Optix Installation Guide |
                    FactoryTalk Optix Runtime setup. For more information about Runtime
                Tools, see FactoryTalk Optix Installation Guide | Runtime
                    Tools.
Can I transfer a runtime license from one device to another?
Yes, you can transfer a runtime license from one device to another device. See FactoryTalk Optix Installation Guide | Rehost a
                    FactoryTalk Optix Runtime entitlement.
Where and how do I create a MyRockwell account?
You can create a MyRockwell account while logged into FactoryTalk Hub. See FactoryTalk Optix Installation Guide | Log in to
                    FactoryTalk Hub.
What are the differences between FactoryTalk Optix Studio and FactoryTalk Optix
                    Pro?
FactoryTalk Optix Studio Pro offers more features than FactoryTalk Optix Studio. To
                see the differences, see FactoryTalk Optix Installation Guide |
                    FactoryTalk Optix Studio versus FactoryTalk Optix Studio Pro.
In which account of my organization do I receive a license?
You first receive licenses in your MyRockwell account. You can then associate the
                licenses with your organization. See FactoryTalk Optix Installation Guide |
                    Entitlements.
Provide Feedback