Features and functionality FAQs
    Where can I find the online help?
The most recent FactoryTalk Optix Help for the current stable FactoryTalk Optix
                release is available at FactoryTalk Optix Help.
How can I find step-by-step assistance for a specific feature? 
You can find step-by-step guides and tutorials for specific features in FactoryTalk Optix Help.
Is it possible to run FactoryTalk Optix Applications on mobile devices?
You can access FactoryTalk Optix Applications with Web Presentation Engines through a
                web browser on your mobile device. See Presentation engines.
Does FactoryTalk Optix Studio provide features for developing applications
                    compliant with CFR21 Part 11?
Yes, FactoryTalk Optix Studio provides features for developing applications compliant
                with CFR21 Part 11. See 21CFR Part 11 Regulation Compliance and the 21 CFR Part 11 Regulation User Guide.
Does FactoryTalk Optix Studio offer automatic project backups?
Yes, FactoryTalk Optix Studio automatically backs up projects that you save and
                retains the last three backups of a saved project. FactoryTalk Optix Studio also
                backs up a  project before you upgrade or downgrade the project. You can use Git
                version control to better manage changes in your projects. See:
How can I be notified when a new version of FactoryTalk Optix is released?
To see released versions of FactoryTalk Optix, see Product Versions - Product Compatibility and
                    Download Center. You can subscribe to new FactoryTalk Optix releases and
                receive automatic emails on Compatibility & Downloads.
What are the new features for the new stable version?
Open the FactoryTalk Optix page in FactoryTalk Hub. Go to FactoryTalk Optix, select your
                organization, and then choose 
Select
. At the bottom of the page, you can open
                the release notes and change log for FactoryTalk Optix. See System features
                in the release notes for a list of new features in the selected version. What are the fixes for the new stable version?
You can review fixes for the new stable version of FactoryTalk Optix by opening the
                release notes for a specific stable version and reviewing the corrected anomalies.
                To see the fixes for the most recent stable version of FactoryTalk Optix, see FactoryTalk Optix Release Notes | Corrected
                    anomalies.
Does Rockwell Automation offer a cloud platform where you can send data?
Yes, see FactoryTalk DataMosaix.
Provide Feedback