Add Edge App Broker to your project
    Ensure that the following items are installed on your system: 
    
    
    
- Edge App Broker
- Edge applications
     TIP: 
    To obtain the Edge App Broker and Edge
        applications, contact your Rockwell Automation representative.
- In your project, right-click the top node, and select .
- Right-clickEdgeApplicationsfolder, and selectEdge App Broker.
- InProperties, configure the Edge App Broker addon.Available Edge App Broker applications depend on what is installed on your system.
- Select models that you want to be available for the broker:- InProperties, select. 
- (optional) Rename the model.
- Next to the model, select. Add Dynamic Link Add Dynamic Link
- From the menu, select the folder you want to use.Rockwell Automation recommends using the contents of theModelfolder for models.
 
Provide Feedback