IUAVariable.RemoteWrite(value, timeoutMilliseconds)
    Writes the value passed in the first argument in the variable on which it invokes. The second optional argument sets the timeout period.
void RemoteWrite(UAValuevalue, doubletimeoutMilliseconds);
Arguments
      - value(UAValue)
- The value to write.
- timeoutMilliseconds(double)
- The timeout period, expressed in milliseconds, after which the API throws an exception.TIP: If not specified, the default value of the argument is30000(30 seconds).
Example
      In the following example, the 
42
 value is written in the Speed
 variable.
        var currentSpeed = Project.Current.GetVariable("Model/Motor/Speed"); currentSpeed.RemoteWrite(42);
Provide Feedback