Manage dynamic links
    Use C# APIs to set or remove dynamic links on the variables. 
The APIs are supplied by the 
IUAVariable
 C# class.
     TIP: 
    By default, dynamic links defined in a NetLogic are read-only,
      whereas dynamic links created with the 
FactoryTalk Optix Studio
 UI are read and write.Provide Feedback