RemoteVariableSynchronizer.Remove(variables)
    Depending on the overload, removes a variable or a list of variables from the 
RemoteVariableSynchronizer
 object on which it is invoked.void public void Remove(IUAVariable variables); void public void Remove(RemoteVariable variables); void public void Remove(IEnumerable<IUAVariable> variables); void public void Remove(IEnumerable<RemoteVariable> variables);
Argument
      - variables(IUAVariable)
- TheIUAVariableC# object to add to the object on which the method is invoked.
- variables(RemoteVariable)
- TheRemoteVariableC# object that identifies a cell of a one-dimensional or multidimensional array to be added to the object on which the method is invoked.
- variables(IEnumerable<IUAVariable>)
- TheIUAVariablelist to be added to the object on which the method is invoked.
- variables(IEnumerable<RemoteVariable>)
- TheRemoteVariablelist to be added to the object on which the method is invoked.
Examples
      In the following example, a variable 
speed
 is removed from the variableSynchronizer
 object.
        variableSynchronizer.Remove(speed);
In the following example, the 
10
 index variable is removed from the variableSynchronizer
 object within the arrayVariable
 array.
        variableSynchronizer.Remove(new RemoteVariable(arrayVariable, 10));
In the following example, the 
10.5
 index variable is removed from the variableSynchronizer
 object within the scalarVariable
 multidimensional array.
        variableSynchronizer.Remove(new RemoteVariable(scalarVariable, new uint[] { 10,5 }));
Provide Feedback