Pull preview
    Pull changes from the remote repository to see conflicts between the local project
      and the remote project.
Pull preview interface

| Item | Description | 
|---|---|
|  | Rows of highlighted conflicts or changes. | 
|  | Select  Take all localto accept all of the local
                changes. Select Take all remoteto accept all of the changes
                in the remote repository. | 
|  | Filter the changes in the preview by displaying  Allproject content, only Updatesto the project, or only Conflictsin the project. | 
|  | Select  | 
|  | Select a conflict to the left in a row to accept the local change.    Local history | 
|  | Select a conflict to the right in a row to accept the remote change.    Remote history | 
|  | An icon in a row indicates:  
 | 
change
preview
conflict
    
Provide Feedback