Rename a role
    Rename a role to change the name of the role to which users are assigned. For example, rename a Supervisor role to Manager role. You can rename one role at a time.
Rename a role from either the dashboard page or 
Project view
.- Either:- Selectand then selectOpen dashboard pageManage user and groups.
- InProject view, expandSecurityandRoles.
 
- UnderRoles, right-click the role to rename.
- SelectRenameand type a new name for the role.To rename a role fromProject view, right-click the role, selectRename, and then enter the new name.
The role is renamed on the dashboard page and in 
Project view
. Provide Feedback