Use translated texts in a string formatter
    Create a reference to a translation key to have the key use the related translated text according to the session locale at runtime. A translation key is a reference to a specific translation in the translation dictionary.
- InFormatproperty, type characters present in the key. The keys containing the typed characters appear.
- Select a key and then pressEnter.
If the text for the key contains placeholders for the string formatter sources, such as “{0}”), the relative properties appear. 
key
string formatter
text
    
Provide Feedback