Change the interface language
    Change the interface language to display a different language throughout the 
FactoryTalk Optix Studio
 application at design time and runtime. - To change the interface language, either:- InProject view, select the project node and then inProperties, expandLocalizationand inLocales, select the language.
- Selectand then in FactoryTalk Optix Studio OptionsLanguage and Locale, select the language. FactoryTalk Optix Studio OptionsLanguage and Locale, select the language.
- Have a different user with a different associated locale language log on.
 
interface language
    
Provide Feedback