System variables
    System variables are automatically created when you create the 
System
 object in a FactoryTalk® Optix™
 project. When you bind a property of a graphic object to a system variable, the system objects in Project view
 appear as categories in the Dynamic Link browser. Each category contains predefined variables:
      
- Application. Variables that provide a blink rate value. These variables determine the number of seconds a value alternates between showing and clearing a value.
- DateTime. Variables that provide current date and time values of the HMI device and allow you to configure date, time, and time zone in the HMI device.
- Display. Variables provide screen brightness, resolution, scale, and orientation.
- Network interfaces. Variables that provide the network settings such as IP addresses for the HMI device.
- WiFi. Variables that allow you to bind to operating mode, network name, security mode, username, password, and access to the LAN network.
system variable
application
date time
display
network
wifi
    
Provide Feedback