Create the System object
    The 
System
 object allows users to view and configure certain system variables, such as the date and time, device, display, and application settings for the FTOptixApplication
.Create one 
System
 object per project.- InProject view, right-clickModeland then select .System1appears inProject view.
system
system object
    
Provide Feedback