Create a button to restart the application
    You must restart the 
FTOptixApplication
 to have date and time changes from the widget take effect. Create a button to restart the 
FTOptixApplication
.- InProject view, right-click the folder to contain the button and select .Button# (type)appears inProject view.
- WithButton# (type)selected, inPropertiesunderEvents, select Add new methodnext to the event, such as aMouseClick event, that you want to restart theFTOptixApplication. Add new methodnext to the event, such as aMouseClick event, that you want to restart theFTOptixApplication.
- ExpandCore commands, selectRestart, and then chooseSelect.
restart
restart application
    
Provide Feedback