Configure session and fallback locales
    Set the session locale to determine the language for text, format or data, and measurement system for values. The session locale at runtime is based on the user locale or the 
Session UI
 object.If there is no locale for the user or 
Session UI
 object, the project uses the first locale in the Locales
 property. Configure fallback locales in case the user-defined session locale is not configured at runtime, or translation is not available for a session locale. - InProject view, select the project node.
- InProperties, expandLocalization, and then inLocales, type one or more locales separated by commas. For example, it-IT, Fr-FR, en-US.TIP:FactoryTalk Optix Studioadds a column in theTranslation Editortable of theLocalizationDictionaryobject for each new locale.
- InTranslation fallback locales, enter additional locales, separated by commas, such as it-IT, Fr-FR, and en-US.
     TIP: 
    At runtime, 
FactoryTalk Optix
 uses the first locale in Locales
 property that is set for the project or the locale that is set for the current user. If the list of locales contains an unsupported locale or a translation is missing the LocalizationDictionary
, the project uses the first fallback locale.Provide Feedback