Time zones in trend graphs
    At runtime, the 
Trend Graphic
 object displays data in the X-axis in the UTC standard time zone. Use the 
Reference time zone
 property of the graph to specify if data displays in the local time zone or the session time zone. When the Trend Graph
 object is connected to a Data logger
, you must enable the Local time log
 property of the application to store data in the local time zone.Provide Feedback