Configure idle timeout for a container
    Apply an idle timeout to a specific container object using a NetLogic. Idle timeouts
      configured using a NetLogic do not apply to the entire project. A timeout can trigger any
      custom event.
- From the toolbar, selectand then search forTemplate LibrariesIdle Timeout
- UnderComponents, dragIdle Timeoutdirectly intoMainWindow (type)or the screen inProject viewwhere you want to display the screen saver.For more information about screens, see Screen.
- InLibraries, selectClose.
- InDuration, enter the time before the timeout occurs.
- InProject view, selectIdleTimeoutLogicand set these values inProperties:- Enabled. Set toTrue
- Duration. Set the idle timeout.
 
- InProject view, expand the importedIdleTimeoutLogicand selectOnTimeout.
- InPropertiesafterOnTimeout, select. 
- In the browser, expandCommands, expand the type of command, and then select the command to execute when the timeout event occurs.
Provide Feedback