Create retentivity storage
    Create a retentivity storage data store to retain data of specific project nodes.
     TIP: 
    For some property values, you can use dynamic links. For more information, see Create dynamic links.
- Create the retentivity storage object:- In theProject viewpane, right-clickRetentivity.
- Select .
- (optional) InProperties, inName, selectto rename the storage. 
 
- Add a project node to retain its data:- InProperties, next toNodes, select. 
- (optional) Selectto rename the node. 
- (optional) Expand the node. InKind, select Set kindand create a dynamic link. Set kindand create a dynamic link.
- (optional) Expand the node. InNodeClass, select the class of the node or selectand create a dynamic link. Add Dynamic Link Add Dynamic Link
 
- Specify how often new data from the selected project nodes is saved by doing one of the following:- InWrite delay, enter milliseconds by selecting. 
- InWrite delay, selectand create a dynamic link. Add Dynamic Link Add Dynamic Link
 
- Determine if you want to retain only the changes that are already stored by doing one of the following:- InDelta observer enabled, set the value.
- InDelta observer enabled, select. Add Dynamic Link Add Dynamic Link
 
retentivity
storage
project node
    
Provide Feedback