Reports
    Use a 
Reports
 object to design, layout, and generate PDF reports. Reports can include data extracted from FTOptixApplication
 and databases. Generate reports from:
      
- FactoryTalk Optix Applicationto include process data and statistical data
- A database to include data recorded by an event logger
Create a report by adding a Reports object to the project.
Apply a stylesheet to a report to customize the appearance of the report. Display information in a report footer to, for example, identify the report, page number, or other pertinent information.
Provide Feedback