Duplicate a recipe schema
    Duplicate an existing recipe schema to base the new schema on the old schema.
- From the toolbar, select.Open dashboard page
- In the editor, selectConfigure a recipe.
- Right-click the available recipe schema and selectDuplicate.
If necessary, edit the duplicated recipe schema. See Edit a recipe schema.
Provide Feedback