Project secrets encryption
    Encrypt secrets in
      projects or use a password that is stored locally in project files.
Requirements
      Encrypt project secrets while
        creating a project. See Create a project.
Encryption scope
      FactoryTalk Optix
:
        - Encrypts passwords in projects.
- Encrypts custom objects with the Password DataType.
- In the projectYAMLfiles, which represent the project information model, replacesValuenodes withSecretValuenodes with encrypted text values.
Projects with encrypted secrets
      FactoryTalk Optix
 handles encrypted projects in the following way: - Opening a project with encrypted secrets when you do not have access to the organization used to create the project or you continue without providing a user password blanks all project secrets.
- Saving an encrypted project as an unencrypted project removes all secrets.TIP: Passwords for user accounts in projects are not considered secrets and are not encrypted with FactoryTalk Hub keys. Passwords for user accounts in projects are securely stored using a hash algorithm.
- Deploying an encrypted project to an unencrypted client displays a warning message. For more information, see Project encryption on a target device.
- Pasting an object from an encrypted project to an unencrypted project blanks the secrets.
- Adding an object to the Template Libraries in an encrypted project blanks the secrets.
- Pasting a password as a text to the clipboard is disabled in encrypted projects.
encryption
    
Provide Feedback