Navigate nodes
    Navigate project content in 
Project view
.- Do any of the following:
- Select any node inProject viewand start typing the name of the node to find.The matching note is selected.TIP: The nodes are searched downward from the currently selected node. If there are no matches, the search continues from the first node to the currently selected node.
- Expand the selected node by pressing.Right arrow
- Collapse the selected node by pressing.Left arrow
- Select the lower node by pressing.Down arrow
- Select the upper node by pressing.Up arrow
- Select the previously selected node by selecting. Navigate backward Navigate backward
- Select the most recent node by selecting. Navigate forward Navigate forward
- Right-click the root project node and then selectCollapse allto collapse all nodes for easier navigation.
- DivideProject viewinto two areas that you can scroll separately. Select Split project viewto divide the view. Select Split project viewto divide the view. Select Split project viewagain to remove the division in the view. Split project viewagain to remove the division in the view.
navigate
    
Provide Feedback