Display information model graphs
    Visualize information models of 
FactoryTalk Optix
      projects in the form of graphs.
     TIP: 
    For more information about project information models, see Information model.
Prerequisites
Install an application that displays graphs 
    
    
DGML
 graphs, such as
        Microsoft Visual Studio with the DGML Editor component. 
     TIP: 
    For more
          information about 
DGML
 files, see Directed Graph Markup Language (DGML) reference - Visual Studio
            (Windows) | Microsoft Learn.- To display information model graphs
- Do either:- InProperties, right-click the property.
- InProject view, right-click the project node.
 
- SelectModel analysisand then select either:- Information model graph (Project only). Visualize only nodes, types, and references related to the user project.
- Information model graph (Ignore OPCUA/Core namespaces). Visualize nodes, types, and references of the user project andFTOptixmodules namespaces, except OPC-UA and Core namespace.
- Information model graph. Visualize all nodes, types, and references of any namespace.
 
Information model graph example

information
model
information model
    
Provide Feedback