Project nodes
    Use 
Project view
 to create and manage nodes and folders in your project.Project view
      Project view
 displays a tree structure comprised of nodes. The nodes are objects and variables organized in folders. Each folder has a dedicated icon and context menu. The context menu displays objects that you can create in that folder. Any subfolder that you create displays the same options as the folder on which it is based. You can create multiple versions of a folder.
     TIP: 
    Search 
Project view
 to find contents without having to navigate and expand folders. Split Project view
 to see multiple areas of the project simultaneously. For more information about the 
Project view
pane, see Project view.Node types
      Project nodes include different object types, object instances, and variables. For more information on how to create, delete, rename, and manage different node kinds, see:
        
project view
    
Provide Feedback