Add collection items to a node
    Add collection items to objects that support them.
     TIP: 
    The available collection items depend on the type definition of the parent object.
Prerequisites
Add nodes to the project. See Add instances of types defined in Companion Specifications.
- To add collection items to a node
- Right-click a node and select .
The collection item appears under the node.
Provide Feedback