Add MQTT Broker
    Configure an MQTT Broker to handle communication between Subscribers and
    Publishers.
- InProject view, right-clickMQTT, and select .
- InProperties, configure theMQTT Brokersettings:- Listener port
- The port number to listen on is required. If this variable is used and no port provided, the default listener is not started.The default forFactoryTalk Optixis a single listener with one common configuration.
- Max connections
- The maximum number of allowed client connections, expressed as an integer, up to 25.
- Max in-flight messages
- The maximum number of Quality of Service (QoS) 1 and 2 messages in-flight per client. This number includes messages that are partway through handshakes and retried. Setting this value to 0 results in no upper limit for these messages. Setting the value to 1 ensures in-order delivery of QoS 1 and 2 messages.
- Max QoS
- The maximum QoS supported. Clients publishing at a QoS higher than the maximum will be disconnected.
- Max queued messages
- The maximum number of QoS 1 and 2 messages in queue per client, not including messages that are currently in-flight (being processed by the broker). Setting a maximum number (greater than 0) of queued messages is recommended.
- Message size limit
- The maximum message size that the broker allows. Received messages exceeding this size will not be accepted by the broker. If you set this value to 0, all valid MQTT messages are accepted without a size limit. However, MQTT imposes an actual maximum size of 268435455 bytes.
- Retain available
- Set tofalseto disable retained message support. If a client publishes a message with the retain bit set, it will be disconnected if the support is disabled.
- Anonymous authentication
- When set toFalse, user-password authentication is required. If set toTrue, no user-password authentication is required.
- Require client certificate
- By default a TLS-enabled listener operate like a HTTPS-enabled Web server: the server uses a certificate signed by a Certificate Authority (CA), and the client verifies if it is a trusted certificate. The overall aim is encryption of the network traffic. Ifyou setrequire_certificateto true, the client must provide a valid certificate to connect to the network. This allows access to the broker to be controlled outside of the mechanisms provided by MQTT.
- CA certificate file
- Defines the path to a file containing the CA certificates. These certificates are trusted when checking incoming client certificates. For CA chain, thecpathis assumed to be hardcoded as\ProjectFiles\PKI\Own\Certs
- Broker certificate file
- Path to the PEM encoded server certificate.
- Broker private key file
- Path to the PEM encoded keyfile.
 
In 
Project view
, in the MQTT
 folder, the configured MQTT broker object appears.mqtt broker
broker
subscriber
publisher
    
Provide Feedback