Configure TLS with client certificate
    
     TIP: 
    The client and server must use the same Certificate
      Authority (CA) for the client and server certificates.
Ensure that OpenSSL is installedon your device.
- In Command Prompt, create a client key by entering:openssl genrsa -des3 -out client.key 2048
- Create a client certificate request using the key:openssl req -new -out client.csr -key client.key
- Use the CA key to sign the client certificate request from step 2:openssl x509 -req -in client.csr -CA ca.crt -CAkey ca.key -CAcreateserial -out client.crt -days 360
Provide Feedback