Deadband interval configurations
    The deadband helps prevent sampling values in rapid succession due to oscillation in the control system.
| Sampling type | Deadband settings | 
|---|---|
| Any change from the previous sample | Default deadband mode= None | 
| Absolute value of change from the previous sample is equal to or greater than a specific value | 
 | 
| Percentage of change from the previous sample is equal to or greater than a specific value | 
 | 
Provide Feedback