Configure the device on which the FactoryTalk Optix Application is running
    Use the Device Settings Widget to configure a device and view product and diagnostic information for the device.
- On the device, open the screen with the Device Settings Widget.If you created your project using theOptixPaneltemplate on the start page, selectSettingsand then selectDevice.
- SelectConfigurationto specify:- Disable application and firmware updates. Select to disable updates or clear to allow updates to the remote device. You must selectRebootto reboot the device after disabling application and firmware updates.
- Device name. Change the name of the device. You must selectRebootto reboot the device after changing the device name.
- Application name. The name of theFactoryTalk Remote Accessdeployed to the remote device.Application nameis read-only.
 
- SelectProduct Informationto view read-only information for the device:- Product name. The name of the device.
- Catalog#. The catalog number of the device.
- OptixPanels firmware. The version number for the firmware installed in the device.
- OS. The version number of the installed operating system.
- System Manager. The version number of the System Manager installed.
- FT Optix Studio. The version ofFactoryTalk Optix Studioused to create the application that is running on the device.
 
- SelectDiagnosticsto view read-only information for the device:- CPU utilization. The CPU utilization of the device.
- CPU temperature. The temperature of the device.
- User memory. The amount of RAM that is utilized.
- Free memory. The amount of RAM that is available.
- Last reboot. The date and time the device was last rebooted.
- Used storage. The amount of disk memory that is utilized.
- Free storage. The amount of disk memory that is available.
- Last deploy. The date and time that aFactoryTalk Remote Accesswas last deployed to the device.
 
- If you disable application and firmware updates or change the name of the device, you must selectRebootto reboot the device and commit the changes.
Provide Feedback