Push a library
    Push a remote library to a remote Git repository to make the changes available to other users of the remote library.
     WARNING: 
    If you use custom 
FactoryTalk Optix Studio
 or FactoryTalk Optix Studio
 beta, pushing library updates to the remote repository prevents other users from pulling the library if they do not use the same FactoryTalk Optix Studio
 release channel.Prerequisites
- To push a library
- From the main toolbar, select.Template Libraries
- SelectPush.Push remote libraryappears, indicating that users with an older version ofFactoryTalk Optixwill be unable to use the library you are about to push until they update their version ofFactoryTalk Optix.
- SelectPush.
- InPush to remote, complete:- Identity. Select your identity. This can be either yourGitLab®orGitHub®identity.
- Owner/Group. Select the owner or group of the repository. This can be either your identity or a group to which you belong.
- Private. Select to create a private repository that only the selected owner or group can associate with a project.
- Public. Select to create a public repository that other owners and groups can associate with a project.
- URL. Displays the URL of the repository based on the selected settings.
 
- SelectPush to remote.TIP: You can manage the remote repository URL and user credentials inFactoryTalk Optix Studio Options. For more information, see Configure version control.TIP: In order to use version control, FactoryTalk Optix library names and repository names must match. The library and repository names must contain only alpha numeric characters, numerals, periods, dashes, and underscores.
The library is pushed to the remote repository.
Provide Feedback