Import fonts
    You can configure your 
FactoryTalk Optix Application
 to use custom fonts in TTF
 or OTF
 format. To use a font other than a default, import the font into the project to make it available as an object property.
     TIP: 
    If you use  folder.
FactoryTalk Optix Studio desktop editor
, instead of performing this procedure, you can copy custom TTF
 or OTF
 font files into the ProjectName
\ProjectFiles\Font- In the main toolbar, select. Browse project files Browse project files
- InProject Files, select. Import file(s) Import file(s)
- Navigate to and select the font to import and then selectOpen.Verify that the font selected for the project is available on the device and supports the required characters.
- CloseProject Files.TIP: To change font family, weight, italic, size, and color, see Style sheet.
The font is now available in the 
Font family
 properties of objects.font
    
Provide Feedback