Apply a global style to the project
    Select a style sheet in which to display the 
FactoryTalk Optix Application
 at runtime.
     TIP: 
      To change style sheets at runtime, see Develop a combo box to pick styles.
Prerequisites
- Configure a global style in a stylesheet. See Configure a style sheet.
- To apply a global style to the project
- InProject view, select eitherNativePresentationEngineorWebPresentationEngine.
- InProperties, inStyle sheet, selectthe style sheet to apply.
The project applies the 
Global Style
 properties from the selected
        style sheet.Provide Feedback