Multistate image
    An object that can have multiple image states based on the input value. Each image state may reference a different image and may have a specific opacity. If the input value does not correspond with any image state, the default value is used (first defined state).
Example
      State 0: 100% opacity

State 1: 50% opacity

State 3: 25% opacity

multistate
multistate image
    
Provide Feedback