Draw an oval or circle
    Use the 
Ellipse
 tool to draw and oval or circle.- InProject view, double-click the container to include the object.
- In the editor toolbar, selectEllipse.
- In the editor, position the crosshair where the oval or circle is to begin.
- Drag to draw the oval or circle.
The object appears in the editor and in 
Project view
.oval
circle
    
Provide Feedback