Draw a rectangle or square
    Use the 
Rectangle
 tool to draw rectangles or squares.- InProject view, double-click the container to include the object.
- In the editor toolbar, selectRectangle.
- In the editor, position the crosshair where the square or rectangle is to begin.
- Drag to draw a rectangle or square.
The object appears in the editor and in 
Project view
.rectangle
square
    
Provide Feedback