XY Chart
    Display the value of two-dimensional variables in a graph.
Use case
      Graphically represent or set machine processes, for example the cutting profile or the work area within which a machine can operate.
     TIP: 
    You can disable the display of a pen by setting its 
Enabled
 property to False
.Example
      
Provide Feedback