Dropdown button
    Button that opens and closes a panel when selected.
Use case
      Open a panel that contains additional options or information when you select the dropdown button.
        
    
    
     TIP: 
    If there is not enough space in width or height with respect to the set opening direction, the panel is opened in the opposite direction. 
Example
      Dropdown button - collapsed

Dropdown button - expanded

Provide Feedback