Circular gauge
    Sets or displays an integer value within a range of possible values.
Use case
      Set and display an analog variable value within a minimum and maximum value.
        
    
    
     TIP: 
    Use the 
Warning zone
 property to display specific ranges of values in different colors.Example
      Circular gauge with two warning zones defined

circular gauge
    
Provide Feedback