Checkbox
    Sets and displays a Boolean value using select and clear.
Operation
      - Selected checkbox
- The associated variable value is True.
- Cleared checkbox
- The associated variable value is False.
Use case
      Enable or disable functions or features within a 
FactoryTalk Optix Application
. For example, toggle a graph that visualizes data.Example
      Cleared checkbox

Selected checkbox

checkbox
check box
    
Provide Feedback