Animation properties
    Configure animations by editing animation properties.
     TIP: 
    For animation examples, download, extract, and open the
      project from AnimationsExample.zip.
Number animation
      A simple animation based on a variable value change over specific time.
| Property | Description | 
|---|---|
| From | Start value of the range | 
| To | End value of the range | 
| Duration | Duration of the animation in milliseconds | 
| Interpolation | The type of interpolation when animation value changes | 
| Target | Target node of the animation | 
| Running | Boolean value | 
| Loops | Number of consecutive animation playbacks. The  -1value sets continuous animation playback. | 
Sequential animation
      Groups of animation executed in a sequential order.
| Property | Description | 
|---|---|
|  Running | Boolean value | 
|  Loops | Number of consecutive animation playbacks. The  -1value sets continuous animation playback. | 
Parallel animation
      Groups of animation executed in a parallel order.
| Property | Description | 
|---|---|
|  Running | Boolean value | 
|  Loops | Number of consecutive animation playbacks. The  -1value sets continuous animation playback. | 
animation
    
Provide Feedback