Align objects
    Align selected objects vertically or horizontally in the Design Area. Aligning objects increases and decreases the margins of the selected items.
- InProject view, double-click a container or select. The editor opens a separate tab. The editor opens a separate tab.
- Select the objects to align.TIP: To select multiple objects, hold downCtrland select multiple objects.
- In the Design Area toolbar, select the icon to align the selected objects in the Design Area: Align at the left border. Align at the left border.
 Aligns at the top border. Aligns at the top border.
 Align at the right border. Align at the right border.
 Align at the bottom border. Align at the bottom border.
 
align
    
Provide Feedback