Delete an event
    Delete a an event to no longer have that event to no longer have the event in the project. The event methods are removed along with the event. 
- Delete all of the methods from an event to delete the event. InProject view, select an object. InPropertiesunderEvents, expand the event. After the method to delete, select.Delete
Provide Feedback